2019-12-18 5:26 AM
I am trying to establish communication between windows 10 and SMT324x9I-EVAL board through USB by setting USB in CDC class.
For starting with, i have used example application given with stm32f4 peripheral library package(en.stm32cubef4\STM32Cube_FW_F4_V1.23.0\Projects\STM324x9I_EVAL\Applications\USB_Device\CDC_Standalone\SW4STM32\STM324x9I-EVAL_USBD-FS).
Unfortunatly, the board is not getting detected in windows device manager and not receiving any interrupts in OTG_FS_IRQHandler.
After enabling VBUS detect, I am receiving OTG_FS interrupt for USB connect and disconnect events but after that no other activity is observed on the USB lines.
Please advice how to proceed further.
Note: JP16 is kept open.
2019-12-18 8:17 AM
Try other examples, double check all jumper, solder-bridge/resistor options.
Try different cables.
Instrument code to output to serial port and check malloc/free usage.
Try building with better tools. Use Keil or IAR evaluations to built the project(s)
2019-12-19 4:37 AM
@Community member Thanks for the response, I have varified all the jumpers and resistors
I have tried flashing this example and few others(Mass storage device examples) with Keil also but still the board is not getting detected in Windows as COM device.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.