2025-01-25 8:55 AM - last edited on 2025-01-28 8:02 AM by mƎALLEm
The conclusion is that setting filters and interrupts on FIFO0 leads to exception handling
FDCAN1_IT1_IRQHandler.
The reason for this behavior is an error in the file. startup_stm32g431cbtx.s
ERROR
..
.word ADC1_2_IRQHandler
.word USB_HP_IRQHandler
.word USB_LP_IRQHandler
.wordh FDCAN1_IT0_IRQHandler
.word FDCAN1_IT1_IRQHandler
.word EXTI9_5_IRQHandler
.word TIM1_BRK_TIM15_IRQHandler
..
This is how it should be
...
.word ADC1_2_IRQHandler
.word USB_HP_IRQHandler
.word USB_LP_IRQHandler
.word FDCAN1_IT1_IRQHandler
.word FDCAN1_IT0_IRQHandler
.word EXTI9_5_IRQHandler
.word TIM1_BRK_TIM15_IRQHandler
...
As an example, the code that I use is for testing so that there are no questions).
void CAN_Config(void) {
FDCAN_GlobalTypeDef *CAN = FDCAN1;
uint32_t *filterRAM = (uint32_t *)RAMBaseFDCAN1;
// Включение тактирования для CAN
RCC->APB1ENR1 |= RCC_APB1ENR1_FDCANEN;
RCC->CCIPR &= ~RCC_CCIPR_FDCANSEL;
// PLL "Q" for FDCAN
RCC->CCIPR |= (0x1 << RCC_CCIPR_FDCANSEL_Pos);
// Init FDCAN module
CAN->CCCR |= FDCAN_CCCR_INIT;
while (!(CAN->CCCR & FDCAN_CCCR_INIT));
CAN->CCCR |= FDCAN_CCCR_CCE;
/*
Baudrate NSJW NBRP NTSEG1 NTSEG2 FDCAN_NBTP (uint32)
125000 1 640 543 95 0x21F5F
250000 1 320 271 47 0x10F2F
500000 2 160 67 12 0x08617
800000 1 100 84 14 0x0540E
1000000 1 80 67 11 0x0430B
*/
// Set the nominal bit timing register
CAN->NBTP = (1 << FDCAN_NBTP_NSJW_Pos) |
(1 << FDCAN_NBTP_NBRP_Pos) |
(66 << FDCAN_NBTP_NTSEG1_Pos)|
(11 << FDCAN_NBTP_NTSEG2_Pos);
// Clear message RAM
for(uint8_t i=0;i< 212;i++){filterRAM[i] = 0;};
/* FDCAN global filter configuration register (FDCAN_RXGFC)
Address offset: 0x0080
Reset value: 0x0000 0000
*/
//CAN->RXGFC = STDfilter_n(2)|EXTfilter_n(0)|ANFS_Reject_rx|ANFE_Reject_rx;
CAN->RXGFC = (2<<16)|(2<<4)|(2 << 2);//
// ID filters 100 and 80
// filterRAM[0] = STDfilterID_DUAL | STDfilterRxFIFO0 | STDfilterID1(0x100) | STDfilterID2(0x80);
filterRAM[0] = (1 << 30) | (1 << 27) | (0x100 << 16) | 80;
// Включить прерывания в FDCAN FIFO
CAN->IE |= 3; // FDCAN_IE_RF0NE_| RF0FE
CAN->ILS |= 1; // RXFIFO0: RX FIFO bit grouping the following interruption
CAN->ILE |= 3; // Enable IT0
// Normal MODE
CAN->CCCR &= ~FDCAN_CCCR_INIT; // Выход из режима инициализации
while (CAN->CCCR & FDCAN_CCCR_INIT);
NVIC_EnableIRQ(FDCAN1_IT0_IRQn);;
NVIC_EnableIRQ(FDCAN1_IT1_IRQn);
}
It took me several hours to understand that someone had screwed up.(
RM0440
Sometimes it blows my mind too))
Solved! Go to Solution.
2026-03-01 10:47 AM
Very good that you corrected this.
You should close this topic and mark your answer as the solution.
The reason why I came to this page in the first place was that Copilot told me that there are errors concerning the CAN IRQ in "some HAL versions".
So artificial intelligence is trained by this forum and now it can simply ignore this posting.
Again:
It is a pity that STM does not care to employ some people who give useful answers here.
All the "Employees" in this forum did not help to solve the problems for which I have visited this forum.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.