2024-07-04 3:29 AM
I'm a fresher as a Firmware engineer. I'm currently working on dataloggers. I'm using STM32U083C-DK board which contains STM32U083MCT6 MCU. I've written the code for the basic functionality of the device i.e sleep and wakeup logic using STM32CubeIDE.
Now, I need to communicate with an external flash memory (W25Q32JVSIQ).
Help me with integrating and modifying the necessary files in the FatFS.
So, after going through some searching, I got to know that I need to integrate FatFS with my project (on STM32CubeIDE) first and then do SPI communication with the W25Q32JVSIQ.
So, till now, I've done these things:
Now, what should I do?
I think, I need to modify the ffconf.h file and Set Up Low-Level Disk I/O Functions.
So, can anyone help me by providing your files for reference or any other references or examples to go through?
2024-07-05 7:21 AM
Hello @RB4020 ,
Welcome to ST Community.
A similar topic has been answered, please refer to this thread: Need to Access External Flash memory as File System
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.