2010-04-24 4:58 AM
F103: quartz selection for mp3 application
#stm32 #stm32-audio-usb2011-05-17 4:48 AM
TLV320AIC23B is a perfect product, exept price ~
5
USD vs less then 1USD for UDA1330ATS:)
even if I will do switching betwin 12.288 and 11.2896 how can I get 48MHz for USB?...
2011-05-17 4:48 AM
Not sure you can do it all with one clock source (absent a good PLL/NCO), codecs like the TI AIC23 had a special USB mode which could use a 12 MHz clock source. While the rates weren't perfect, they might be close enough. I think I used a source capable of switching between 12.288 MHz and 11.2896 MHz.
http://focus.ti.com/lit/ds/symlink/tlv320aic23b.pdf8000
11025 16000 22050 32000 44100 480002011-05-17 4:48 AM
STM32F105 family does not have memory interface. I use NAND.
Another quastion: the accuracy of HSI is +-1%. Is it anougth for USB?
In my board I also have RTC quartz and can trim HSI if nesessary, should I do it?
2011-05-17 4:48 AM
Hi,
To run USB on our STM32F103 devices , exact 48MHz is needed for USBCLK which is drived from SYSCLK after PLL. Thus SYSCLK should be either 72MHz or 48MHz. I would recommand you to use STM32F105 device from our connectivity line offer which is the best fit for your application : Audio + USB . A special Audio PLL is implemented and allows you a wide choice for Audio sampling rates, you can refer to our on-line presentation for more details :http://www.st.com/stonline/domains/support/epresentations/stm32connectivity/stm32connectivity.htm
Cheers, STOne-32.2011-05-17 4:48 AM
Hi,
Regarding HSI, it is not enough to cover all cases, USB Clock jitter at 48MHz should not exceed absolute ''0.25%'', But it can work in your application for enumeration. However If you try to perform electrical testing , it may violate the USB specs. Cheers, STOne-32.2011-05-17 4:48 AM
As far as I see trimming may be used. The step of trim is 40kHz. 0.25% means window 120kHz. So I think it is possible, I'll make experiment.
thanks
2011-05-17 4:48 AM
You'd probably have to actively discipline it rather than just trim an forget. It is likely to change with voltage supply and temperature (not stable). The 40KHz LSI is certainly all over the place compared to an 8MHz TCXO
Given how easy a digital NCO (DDS) could have been implemented, It's kind of a pity that the STM32 doesn't have a handful.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.