2019-07-01 3:22 AM
I' m working on an stm32F429discovery board and I want to read an image from an USB stick
I initialized the USB stack, registered the MSC class and started the USB. Really CubeMX did it for me calling MX_USB_HOST_Init() and FAT_FS_init at the beginning.
In USBH_UserProcess() (called by INT when the USB stick is put on ) I called f_mount and having the _FS_REENTRANT=1 it tries to call a semaphore and at this point everything freezes.
I'm using FreeRTOS an the 1st thing I did is to increase the size of the stack but nothing changes and indeed I don't think it's a problem of size but must be something connected to the semaphore and to the INT and I don't understand.
Any idea?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.