2025-04-04 7:35 AM - last edited on 2025-04-04 7:57 AM by STTwo-32
@STTwo-32, I also noticed issues in the EXTI.
Sample:
stm32h7s7xx.h, &(EXTI->PR1) == 0x58000088
STM32H7S.svd, &(EXTI->PR1) == 0x58000020
When should we expect the upcoming release (in 2 month?)?
Also, are there public script which validate that stm32*.h and .SVD do match?
Solved! Go to Solution.
2025-04-04 8:11 AM - edited 2025-04-04 8:11 AM
Hello @Marc_LM
I've escalated this internally for correction (under internal ticket number 206865). Unfortunately, I don't have visibility on the exact date for the correction. For a Script that validate that stm32.h and. SVD do match, there is not such a public script.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-04 8:11 AM - edited 2025-04-04 8:11 AM
Hello @Marc_LM
I've escalated this internally for correction (under internal ticket number 206865). Unfortunately, I don't have visibility on the exact date for the correction. For a Script that validate that stm32.h and. SVD do match, there is not such a public script.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-04 8:50 AM
Previously:
https://community.st.com/t5/stm32-mcus-embedded-software/fixes-for-stm32h743-svd/m-p/774952
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.