2020-08-06 8:00 AM
In order to evaluate emWin graphics library, I'm using the evaluation board STM32H745I-DISCO and I'm trying the example project "STemWin_HelloWorld".
When I call GUI_DispStringAt ("hello",0,0) I see that the string is not displayed from X = 0 position, but from an X offset of some pixels. Also the "STemWin_SampleDemo" example project have all the windows that start from an offset from the left of display. What could be the problem?
Thanking in advance,
Massimo Badanai
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.