2016-12-26 8:51 AM
hi all.
running the demonstrations project on STM32F4X9-EVAL on the EVAL board works fine.
in my project i need to conserve power so i need to go into stop,ode while system is idle.
stop mode will require GUI_Exit() and GUI_Init() again and again. here is where i run into problem. first init sequnce goes OK, but after applying GUI_Exit() and then GUI_Init() - system runs into hard fault during init.
tried to run the subject project with minor change :
int main(void)
{
/* STM32F4xx HAL library initialization:
- Configure the Flash prefetch, instruction and Data caches
- Configure the Systick to generate an interrupt each 1 msec
- Set NVIC Group Priority to 4
- Global MSP (MCU Support Package) initialization
*/
HAL_Init();
/* Configure the system clock to 180 MHz */
SystemClock_Config();
/* Enable CRC to Unlock GUI */
__HAL_RCC_CRC_CLK_ENABLE();
/* Initialize GUI */
GUI_Init();
HAL_Delay(10);
GUI_Exit();
HAL_Delay(10);
/* Initialize GUI */
GUI_Init(); - HARD FAULT HERE.
.
.
.
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
tried the same on STeMwin 'Hello World' project - it runs fine.
trying to figure out what's the differences between those 2 projects and the cause for that problem
P.s : matched clock speed to 168 MHz, at both projects.
examples were taken from CUBE V1.13
Thank You.
#emwin #rtos #freertos #low-power2016-12-29 5:41 AM
HI again
just to clarify:
i'm running 2 projects which include STemWin. one include freeRTOS and named 'Demonstrations', the other is stand alone and named 'Hello World' at those two projects i run the above code. the one with freeRTOS fails.
there are different libraries for OS and none OS.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.