2019-04-15 7:28 AM
If you are compiling the Cube-drivers with the flags: USE_HAL_DRIVER and USE_FULL_LL_DRIVER, and you are including an LL.c-file in your file list (e.g. stm32h7xx_ll_rcc.c) you will get:
stm32h7xx_ll_rcc.c:27:0: error: "assert_param" redefined [-Werror]You get this error because the code:
#ifdef USE_FULL_ASSERT
.............
#else
#define assert_param(expr) ((void)0U)
#endifis included in both the configuration header file: stm32h7xx_hal_conf.h (which is the mandatory configuration file based on the template file supplied in the HAL library) and in every LL.c-file (such as stm32h7xx_ll_rcc.c, stm32h7xx_ll_usart.h, etc.).
Is there a suggested work-around to avoid the redefinition of "assert_param"?
2024-01-15 1:26 AM
Hello ST
Nearly 5 years after, the bug is still present!!! Cannot compile F4 project with HAL and LL driver.
Your are not testing the firmware package you release... really bad way of work, but ok. We know that we have to make the testing that you do not do.
But could you at least correct the but that are reported by users!!!!!!
Just do your job please
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.