2020-10-01 4:05 AM
Hello, I'm testing RTOS Message queue on STM32F7,
When I try to create an message queue to send an message from Thread 1 to another thread, my data I receive in target Thread is unstable.
For example, I'm trying to send uint16_t 317, but in target Thread sometime is 0, and sometime exactly 317.
Anyone can tell me what happened?
Below is my function
// Define handle
QueueHandle_t MsgHandle;
// Define new queue
osMessageQDef(myQueue02, 16, uint16_t);
MsgHandle = osMessageCreate(osMessageQ(myQueue02), NULL);
// Put a message
uint8_t *data = "abcxyz";
uint16_t FlashDataSize;
FlashDataSize = (int)strlen(data);
osMessagePut(MsgHandle, FlashDataSize, 0);
// Get a message
osEvent size_event;
size_event = osMessageGet(MsgHandle, 0);
// => size_event.value.v = ?? unstable (= 0 or = 317 (correct))Many thanks,
Hieu
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.