2020-08-29 3:09 PM
Hello
I am trying to perform FFT on real data sampled with ADC
However, first I need to perform it on test data that I generated inside my code to verify it would work
then I generated 50hz sine + 150hz sine like this
Note that buffer is int16, signed two's complement 16 bits;
NOW
rfft_q15 expect 1.15 format...
where 1 (msb) is sign and 15 are fractional (so much like two's complement)
I am not interested in exact values of Fourier Transform, rather I want to determine which bins have highest value, SO I JUST COPIED THESE VALUES TO q15_t BUFFER AND FED INTO arm_rfft_q15
As for the output, now it gives back 9.7 where 9 bits are integer parts and 7 bits are fractions. Since I do not care about exact values and just want to know which frequency bin has biggest absolute value I ignore these bits
Now what I though was following: if msb of 9 bit integer is actually kind of the sign bits and it works like two's complement. I should be able to store it in int16 and just pick up greatest value
However it didn't work, rfft output didn't make any sense.
is it because that q15 format does not actually work like two's complement and sign bit is just literally to carry information about the sign?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.