2017-03-01 1:34 AM
Hi.
I designed a PCB to use stm32f407 and TLV320AIC12 codec for capturing and playing sound.
As you can see I connected I2S pin of stm to tlv in this way:
STM32F407 TLV320AIC12
CK---------------------------->SCLK
WS--------------------------->FS
ext_SD---------------------->Dout
SD---------------------------->Din
MCK-------------------------->MCLK
and also I connected INP to microphone and OUTP1 to speaker.
I used stmcube software for configure my application, so I wrote my code in the following format and started speaking in microphone but I could not hear any voice from speaker.
I do not have any idea why it is not working.
thank you for guiding me in advance.
//*******************************************************************
MX_I2S2_Init();
uint8_t CnvRx[50]; uint16_t Txbuff[5]; uint16_t Rxbuff[5]; while(1) { Txbuff[0]=Rxbuff[0]; //DAC input data Txbuff[1]=0x0000; HAL_I2SEx_TransmitReceive(&hi2s2,Txbuff,Rxbuff,2,100); sprintf((char*)CnvRx,'%04X,%04X\n',Rxbuff[0],Rxbuff[1]); Debugger_Send_Data(CnvRx);//send data out by uart }DebuggerOutput:
000F,0000
0010,0000000D,8000000E,0000000E,8000//*******************************************************************
#stm32f407 #tlv320aic12 #codecWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.