2025-03-21 12:33 AM
I have 3 boards of stm32 customized board
From one board iam using uart to flash IAP code and application code.
By uart I take data for other data and transmit through CAN PROTOCOL and that data (application code) I need to flash code to the other board .is it work or not
By can communication
Is it work
Plz help me
2025-03-21 5:09 AM
Hello @Saichandu29
Please refer to this post.
Also refer to the AN3154 to develop your bootloader host using CANBUS.
2025-03-21 5:19 AM
You can use FDCAN to communicate with an STM32H7 board and use the information however you like, including to do IAP. The system bootloader also supports FDCAN.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.