2017-03-08 6:51 AM
Hi
I have a custom bootloader that I flash to the first sector (0x8000000) and when it receives a new program it loads it to 0x8003000. I can jumps to the user application,and also
jumps
from user application to the bootloader.I
want to know if there
are any methods to tell the custom boot
loader
, there are not a simple start-up, but it's a jump from user application.
can i share a variable between bootloader and user application?
Thank you in advance !
#custom-bootloader #stm32f12017-03-08 7:33 AM
You'd need to carve out an area of RAM, which you app doesn't clear, where you can place variables or a structure, to communicate data between them
typedef struct _FOO {
int a;
int b;
} FOO;
FOO *foo = (FOO *)0x2000FF00; // some upper RAM area for your part, pick something appropriate
foo->a = 1234;
foo->b = 4321;
2017-03-08 9:05 AM
should i do that in my custom bootloader?
typedef struct _FOO {
int a;
int b;
} FOO;
FOO *foo = (FOO *)0x2000FF00;
if (foo->a == 1234) // thats mean i was in application
{
//do ......
}
Thank you
2017-03-08 9:11 AM
The CPU doesn't inherently clear RAM over a reset, so the technique is viable either way. The example assumes your part has 64KB of SRAM, and you hide 256 bytes from the linker so you can pass parameters. This could be a command line, or whatever.
2017-03-08 10:14 AM
How can i choose the adresse
0x2000FF00, should be before the bootloader or in application memory?
thnak's
2017-03-08 11:18 AM
It will depend on the specific part you are using. The boot loader and application share the same RAM resources, the linker settings typically assume they can use all available memory.
2017-03-09 4:05 AM
I chosed 0x200001DC as an adresse for FOO, but when i jump from user application to bootloader 'foo->a' and 'foo->b' equals zero, so foo->x change when i jump. any suggestion
thank's
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.