2015-08-18 6:20 AM
I think I found a bug in STM32CubeL1 in function
HAL_RCC_GetSysClockFreq(). Clock settings are: &sharpdefine HSE_VALUE ((uint32_t)12000000) // external oscillator at 12 MHz /* Enable HSE Oscillator and Activate PLL with HSE as source */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL8; //RCC_PLL_MUL12; RCC_OscInitStruct.PLL.PLLDIV = RCC_PLL_DIV3; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2 clocks dividers */ RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2); RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK) { Error_Handler(); } So I expected a SystemCoreClock = 32000000. But instead HAL_RCC_GetSysClockFreq() returned 24000000. It turns out that parentheses are wrong in the following section of HAL_RCC_GetSysClockFreq(): /* HSE used as PLL clock source */ pllvco = HSE_VALUE * (pllm / plld); // HSE_VALUE = 12000000, pllm = 8, plld = 3 After changing into pllvco = (HSE_VALUE * pllm) / plld; it returns 32000000 as expected. This is because in the incorrect version above 8/3=2,6666 and the remainder is dropped, so 12MHz*2=24MHz! #stm32cubel12015-08-19 2:03 AM
Hi sciro,
Thanks for your feedback. The issue has been reported internally.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.