2019-05-06 4:01 PM
I noted that when I call HAL_GPIO_DeInit is called (stm32h7xx_hal_gpio.c v1.4.0) the wrong External Interrupt get's de-initialized. After investigating further and comparing to the previous version I noted the following in the external interrupt de-init block: Everywhere the pin mask:
0x0FUL << (8U * (position & 0x03U))
appears, it should be changed to:
0x0FUL << (4U * (position & 0x03U))
like it was originally.
/*------------------------- EXTI Mode Configuration --------------------*/
/* Clear the External Interrupt or Event for the current IO */
tmp = SYSCFG->EXTICR[position >> 2U];
tmp &= (0x0FUL << (8U * (position & 0x03U))); // <-- Incorrect Here
if (tmp == (GPIO_GET_INDEX(GPIOx) << (8U * (position & 0x03U)))) // <-- Incorrect Here
{
tmp = 0x0FUL << (8U * (position & 0x03U)); // <-- Incorrect Here
SYSCFG->EXTICR[position >> 2U] &= ~tmp;
/* Clear EXTI line configuration for Current CPU */
EXTI_CurrentCPU->IMR1 &= ~(iocurrent);
EXTI_CurrentCPU->EMR1 &= ~(iocurrent);
/* Clear Rising Falling edge configuration */
EXTI->RTSR1 &= ~(iocurrent);
EXTI->FTSR1 &= ~(iocurrent);
}
Solved! Go to Solution.
2019-05-08 1:56 AM
Hello @Martin Franke ,
This reported issue is confirmed and will be fixed in the coming release of CubeH7.
Thank you for highlighting this.
Regards,
Imen
2019-05-07 5:49 AM
Hello @Martin Franke ,
We will check this internally and come back to you soon with update.
Regards,
Imen
2019-05-08 1:56 AM
Hello @Martin Franke ,
This reported issue is confirmed and will be fixed in the coming release of CubeH7.
Thank you for highlighting this.
Regards,
Imen
2019-05-08 8:25 AM
Hello @Imen DAHMEN
Thank you for verifying this so quickly!
Regards,
Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.