2020-02-04 10:36 PM
File: RootProject\Middlewares\ST\STM32_USB_Host_Library\Class\HID\Inc\usbh_hid_keybd.h
#define KEY_CAPS LOCK 0x39
2020-02-04 10:50 PM
You did not tell us which STM32 model, but indeed, I just went randomly to https://github.com/STMicroelectronics/STM32CubeL4/blob/master/Middlewares/ST/STM32_USB_Host_Library/Class/HID/Inc/usbh_hid_keybd.h and lines 106, 110 and 124 all contain the same bug, so I guess this goes across all/several Cubes.
JW
@Amel NASRI
2020-02-05 12:36 AM
Hello @Community member & @rtek1000 ,
Thanks for bringing these errors to our attention. Adding @Ons KOOLI on the loop to take required actions.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-02-07 6:43 AM
Hello all,
Thank you for mentioning this.
This will be fixed soon for USB Host library.
Regards,
Ons.
2020-02-07 7:42 AM
Thanks, Amel and Ons.
JW
2020-02-07 4:39 PM
Thank you for your attention!
About the USB Host library: Is there any example of use for the HS and FS ports independently with the use of RTOS, or without the use of RTOS?
I tried to use the two ports independently, the USB HS with a pendrive (MSC) and the USB FS with a keyboard (HID), but I couldn't.
It only works if the ports are treated in sequence, but not in parallel.
From what I could see, the HAL libraries are shared, the two ports use the same HAL functions.
The same goes for other hardware, such as SPI, I2C etc.
Thank you.
2020-02-14 2:08 AM
Hi rtek1000,
Could you please transform this comment into a new question in the forum?
Making the necessary tags will help you get a faster dedicated answer.
Thank you,
Ons.
2020-02-19 11:36 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.