STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

dual Micro SD in one Mass Storage Device

hii need help to have dual Micro SD in one Mass Storage Device in H743 for see two micro sd in pc from one usbproject use two sdio 1 & 2 , devise fs and mass storageit work correct for every micro sd separately but not work together in code last init...

MacLaren by Associate III
  • 2092 Views
  • 4 replies
  • 0 kudos

Resolved! VCONN_SUPPORT

I would like to enable VCONN based on STM32CubeExpansion_USBPD_F0_V2.1.0.I found CMACRO "_VCONN_SUPPORT", but I encountered complile errors below if I used _VCONN_SUPPORT.compiling usbpd_dpm_core.c...../../../../../../Middlewares/ST/STM32_USBPD_Libra...

Using USB Vendor ID from ST

Hello together,We planned to use for our product the following MCU: STM32L4A6RG.So is it possible to use the USB Vendor ID from ST if I implement in the Firmware a Virtual COM Port over USB interface? I know that I can use the USB VID for evaluation ...

DMark by Associate II
  • 2786 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.