2025-01-26 11:43 PM
According to manual below, function should SEND out a SOLICIT message.
Function returns NX_SUCCESS (0x00) means SOLICIT message successfully sent.
Actually code, after some checks, just set nx_dhcpv6_state variable in DHCPv6 to NX_DHCPV6_STATE_SENDING_SOLICIT value and returns ALWAYS NX_SUCCESS, regardless of what DHCPv6 thread will do.
Therefore we will get NX_SUCCESS before actual sending the SOLICIT packet and even if this packet is not sent at all by DHCPv6 thread for any reason, e.g. no packets available in packet pool.
Also very critical, there is no high level function that user can use yo check for status end errors in DHCPv6 thread, no way to implement correctives actions unless to access global variables and void any quality certification.
Send a SOLICIT message
UINT nx_dhcpv6_request_solicit(NX_DHCPV6 *dhcpv6_ptr);
This service sends a SOLICIT message out on the network. If the message is successfully sent, a successful status is returned. A successful completion does not mean the Client received a response or has been granted an IPv6 address yet. The DHCPv6 Client thread task waits for a reply (an ADVERTISE message) from a DHCPv6 Server. If one is received, it checks the reply is valid, stores the data to the Client record and promotes the Client to the REQUEST state.
Note: If the Rapid Commit option is set, the DHCPv6 Client will go directly to the Bound state if it receives a valid Server ADVERTISE message. See the service description for nx_dhcpv6_request_solicit_rapid for more details.
dhcpv6_ptr: Pointer to DHCPv6 Client instance
NX_SUCCESS (0x00) SOLICIT message successfully sent
NX_PTR_ERROR (0x16) Invalid pointer input
NX_CALLER_ERROR (0x11) Must be called from thread
Threads
2025-01-27 2:18 AM
Hello @mbarg.1 ,
what tests you did that confirm this statement :
"Therefore, we will get NX_SUCCESS before actual sending the SOLICIT packet and even if this packet is not sent at all by DHCPv6 thread for any reason, e.g. no packets available in packet pool."
did you see status return set to success without any request sent?
also, I think that a correct calling flow will ensure that DHCP start is executed correctly before calling the solicit function.
see the example netxduo/samples/demo_netxduo_dhcpv6_client.c at master · eclipse-threadx/netxduo · GitHub
for more details.
Regards
2025-01-27 4:24 AM
I can confirm that I discovered this bug because I did THIS mistake in my code:
did not initialize packet pool.
Now, DHCPv6_create() and DHCPv6_start executed with nx_dhcpv6_request_solicit, as well as nx_dhcpv6_request_solicit(), but no packet were sent out from interface.
To double check bug, I initialized correctly the packet pool, used all packets in the pool for other functions, than call nx_dhcpv6_request_solicit() and again I got nx_dhcpv6_request_solicit but no packet were sent out of interface and no error was reported anywhere.
2025-01-27 4:44 AM
The problem come from _nx_dhcpv6_process() function that does not return errors and ignores errors in called functions.
In case NX_DHCPV6_STATE_SENDING_SOLICIT:
@line 3830:
/* The caller has requested to send a solicit message. */
case NX_DHCPV6_STATE_SENDING_SOLICIT:
{
dhcpv6_ptr -> nx_dhcpv6_message_hdr.nx_message_type = NX_DHCPV6_MESSAGE_TYPE_SOLICIT;
dhcpv6_ptr -> nx_dhcpv6_solicitations_sent++;
/* Send the DHCPV6 Solicit message. */
status = _nx_dhcpv6_send_request(dhcpv6_ptr);
/* Check for error. */
if (status != NX_SUCCESS)
{
/* Return. Can't do any more now. */
return;
}
..........
Obviously thread tries again and again but if empty or invalid pool condition is not cleared, packet are not sent; on other side, application cannot be informed that we have a proble and we are stuck in infinite loop.
2025-01-31 5:41 AM
Hello @mbarg.1 ,
I agree with you on booth points just if you can mention the MCU platform you are using and which package you're getting Azure ecosystem packages is it from X_cube_azure_xx firmware package or on the CubeFirmwareH5 package which natively supports Azure.
Regards
2025-02-01 4:31 AM
AZRTOS is 3.3 - NetXDuo is 6.4 - STM32CubeIde is 1.17 - board I use as reference is NUCLEO-H743ZI/NUCLEO-H743ZI2 - H7 Fw 12.1.1
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.