STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TouchGFX with USB cdc Host

Hello everyone,I am developing firmware for the STM32F7469I discovery board, and I'm utilizing TouchGFX for the GUI aspect of the project. However, I am encountering a problem when enabling USB-FS HOST functionality. The GUI and other peripherals suc...

Usb host with touch gfx

Hi everyone..I am using USB host for communication CDC along with touch GFX for grafix which will use RTOS, The usb is not getting ready after the start state of usb what will be the issue, but when I configure only USB CDC HOST with out touch GFX it...

FMC gives no output for LCD

Hello,Apologies if this is posted in the wrong location. I am trying to control an LCD (ST7789) with my STM32U5G9J-DK2 using FMC. In CubeMX, I configured the NOR Flash/PSRAM/SRAM/ROM/LCD 1 to use NE1 and A0 with 16 bits of data. I also ensured to con...

STL Flash test failed

Hello,I'm working to add the STL Library to my existing project, I'm trying to run the function StlSingleTest but it fails (STL_FAILS) executing the STL_SCH_RunFlashTM(&StlFlashStatus) section.micro: STM32F446ZETFlash:Bootloader: 0x08000000 - 0x0800F...

MauroM by Associate
  • 2936 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 FATFS with SPI FLASH

I am trying to interface a SPI flash from Winbond (W25Q64JV) with FATFS.I have no previous experience with FATFS.I initialize FATFS in CubeMX with the option "used-defined" and modified the MAXIMUM and MINIMUM Sector Size to 4096, as it is the smalle...

STM32L432 LPTIM prescaler behaviour

I have a NUCLEO-L432KC that I am trying to configure such that a LPTIM interrupt fires at a set time period in the future. To simplify calculations, the future time is 2048 low frequency clock ticks away (62.5 ms).I can achieve this with relative sim...

JordanY_1-1738124750443.png JordanY_2-1738124998826.png
JordanY by Associate II
  • 5536 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.