2025-12-11 8:23 AM - last edited on 2025-12-11 8:38 AM by Andrew Neil
Split from STM32G431CBU: section `.bss' will not fit in region `RAM' as that issue is solved, and this is a new question.
One more question. If you can help.
BSP_TS_Init e BSP_TS_GetState is not recognized in IDE versions 1.19 and 1.20.
Therefore, TOUCH doesn't work.
BSP_TS_Init(ILI9488_TFTHEIGHT, ILI9488_TFTWIDTH);
BSP_TS_GetState(& osc->touchScreen);
What did I forget to port?
Solved! Go to Solution.
2025-12-11 1:21 PM
I managed to solve it. OK now.
I was having problems with the "stm32_adafruit_ts.c" file.
Code successfully ported to the G431. Only a slight flickering on the display due to low memory.
I didn't give up until I succeeded.
Thank you.
2025-12-11 8:40 AM
What do you mean by, "not recognised" ?
Is this just within the Editor, or an actual build error?
Does your project contain definitions for those functions?
2025-12-11 1:21 PM
I managed to solve it. OK now.
I was having problems with the "stm32_adafruit_ts.c" file.
Code successfully ported to the G431. Only a slight flickering on the display due to low memory.
I didn't give up until I succeeded.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.