STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is UM1884 (STM32L4/L4+ HAL and low-layer drivers UM) description for RCC_PLLInitTypeDef inconsistent with header file 'stm32l4xx_hal_rcc.h' generated by STM32CUBEMX with respect to PLLP, PLLR parameter definitions?

The structure definition for RCC_PLLInitTypeDef in the header file 'stm32l4xx_hal_rcc.h', generated by STM32CUBEMX, is inconsistent with the RCC_PLLInitTypeDef struct description in the STM32L4/L4+ HAL and low-layer drivers UM (UM1884 Rev8) page 821,...

Tritc.1 by Associate
  • 1833 Views
  • 1 replies
  • 0 kudos

HAL_Program_Flash not writing

Hello! I'm using the STM32F767ZI Nucleo board. I'm trying to test an IAP using LwIP. Since I can only get LwIP working in a FreeRTOS environment., that's what I'm using, I have the following code which I cannot get to even do a simple mass write of F...

HAL_SPI_Transmit_IT blocks

Hello,I've a problem with HAL_SPI_Transmit_IT() function as it blocks similar to HAL_SPI_Transmit.Microcontroller: STM32F205VCT6Compiler: arm-none-eabi-gcc, gcc version 7.3.1 20180622 (release)[ARM/embedded-7-branch revision 261907] (15:7-2018-q2-4)C...

0690X000006CGEWQA4.png 0690X000006CGEbQAO.png
Marc1 by Associate III
  • 10342 Views
  • 17 replies
  • 0 kudos

Resolved! Best Practice For Updating Custom Bootloader

I have a bit of an interesting situation. Our boards utilize the STM32f769NI chip, and we run our own custom bootloader that is used to read firmware images off of a microSD card and then update the firmware in flash memory. We flash a bootloader to ...

BJohn.1 by Associate II
  • 2385 Views
  • 1 replies
  • 0 kudos

Resolved! Has anyone else noticed a typo in stm32g4xx_ll_tim.h in the cube. TIM_CR1_CMS_0 is the center-down.

#define LL_TIM_COUNTERMODE_CENTER_UP          TIM_CR1_CMS_0       /*!< The counter counts up and down alternatively. Output compare interrupt flags of output channels are set only when the counter is counting down. */#define LL_TIM_COUNTERMODE_CENTER...

USB to Serial data loss on STM32F777BIT6 (Works fine on Windows7, randomly loses data on Windows10)

Hi,I am using an STM32F777BIT6 in USB to Serial mode.Everything works fine except for a random loss of data on the windows side.After weeks of frustration I found the cause of this problem: Windows 10 CDC driver for virtual com ports. I tried the pr...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.