STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Transfer project to new board

Hello!I have a education task. I need to transfer X-CUBE-USB-AUDIO (https://www.st.com/en/embedded-software/x-cube-usb-audio.html) to stm32f746g discovery. Project supports boards STM32446E-EVAL and 32F769IDISCOVERY. I think stm32f746g is similar 32F...

VGuly.1 by Associate
  • 1448 Views
  • 2 replies
  • 0 kudos

Resolved! Where do you log bugs discovered in the `HAL_`?

I believe I have found a bug in `HAL_I2C_Master_Transmit`.The timeout parameter begins counting from the instant the transaction begins, and it doesn't appear that the watchdog is being reset with each incoming byte. Therefore, when you have a long I...

0693W000005ArrIQAS.png
Zak by Associate II
  • 1729 Views
  • 2 replies
  • 0 kudos

ST USB DFU bootloader problem

Hi!I'm using CubeMX USB DFU bootloader on STM32F103C8T6 chip. For some reasone example takes itself 48 kB of flash, but don't use even half of it.So i changed USBD_DFU_APP_DEFAULT_ADD from 0x0800C000 to 0x08008000 and changed FLASH_DESC_STR  to  "@In...

DM.1 by Associate
  • 1337 Views
  • 1 replies
  • 0 kudos
HPére.1 by Associate
  • 1341 Views
  • 0 replies
  • 0 kudos

Data Corruption with USB CDC communication

Continuous transmission of data of tx rate 500 samples per seconds(33 bytes per sample) using USB virtual com port(USB CDC).USB mode - full speedTransmit data to serial monitor using function CDC_Transmit_FS();Received data on serial monitor is corru...

Aishwarya by Associate III
  • 1636 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.