STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Changing the ThreadX timebase to 1ms

Due to more performance requirement, i wanted to change the ThreadX timebase to 1ms. To what i have researched till now i need to make the following #define TX_TIMER_TICKS_PER_SECOND to 1000 which is usually set at 100 which is 10ms. Any idea what el...

data sharing between the cores

Hi,I'm using STM32H7 dual core, where the data has to be shared between the cores, so im having totally 21 variables totally 76 bytes, thought of do it like a structure, so where to place the structure exactly for this data sharing. so, this structur...

Cube/USB/CDC / bulk endpoints overlap?

Hi!EDIT: WARNING! This is no real fix... The bug remains...With STM32Cube_FW_F2_V1.9.0 and CDC's /dev/ttyACM0 I had funny glitches on VoidLinux, when i tried full duplex communication (host<>device):some packets never arrived at the USB hostsome shor...

RRIDDICC by Associate III
  • 548 Views
  • 2 replies
  • 1 kudos

Resolved! STM32H747IIT6 ETHERNET RMII PROBLEM

Hello,I am using the STM32H747IIT6 microcontroller along with the LAN8742A Ethernet PHY, configured in RMII mode. However, I am facing issues where the Ethernet interface is not working at all in my circuit. It appears there may be multiple bugs or c...

KAnahar by Associate III
  • 3265 Views
  • 6 replies
  • 1 kudos

PDM2PCM(HP) library details

Good morning, if possible, I would like more details about the following PDM2PCM(HP version) library used for converting PDM data to PCM.           typedef struct{ uint16_t bit_order// MSB / LSB uint16_t endianness;// big endian / little endian uint3...

Mavi by Associate II
  • 1722 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.