2025-12-15 3:17 AM
Hi,
I'm using STM32H7 dual core, where the data has to be shared between the cores, so im having totally 21 variables totally 76 bytes, thought of do it like a structure, so where to place the structure exactly for this data sharing. so, this structure should be placed in any linker file of one of the cores or where?
if so, thus we have to keep the structure in both the core or what
which method is a fastest wat to share the data, like a ring buffer, HSEM.
if we use HSEM, we can use that structure or access outside, before calling the HSEM TAKE, or structure values should be assigned only inside after the HSEM TAKEOVER.
regards,
srinath
2025-12-15 3:20 AM - edited 2025-12-15 3:27 AM
Try a search of the Knowledge Base
PS:
Also check out the available Application Notes; eg,
AN5617: STM32H745/755 and STM32H747/757 lines inter-processor communications
via: https://www.st.com/en/microcontrollers-microprocessors/stm32h7-series/documentation.html
2025-12-15 3:34 AM
@Andrew Neil wrote:
Also check out the available Application Notes; eg,
AN5617: STM32H745/755 and STM32H747/757 lines inter-processor communications
via: https://www.st.com/en/microcontrollers-microprocessors/stm32h7-series/documentation.html
+ Check the OpenAMP examples: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H747I-EVAL/Applications/OpenAMP
2025-12-15 3:42 AM - edited 2025-12-15 3:45 AM
@Srinath_03 which also shows up in the Knowledgebase search results ...
PS:
More on OpenAMP (Open Asymmetric Multi-Processing):
https://www.openampproject.org/
https://github.com/OpenAMP/open-amp
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.