STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What's the best way to port CMSIS UART from F0 to G0

An existing project runs on STM32F091, it use CMSIS USART driver (ARM_DRIVER_USART Driver_USART1). Now I need to migrate this project to run on STM32G070. But in CubeMX for STM32G070, there aren't any USART driver under CMSIS driver, except a header ...

TDao.19 by Associate II
  • 7007 Views
  • 17 replies
  • 0 kudos

Resolved! Bug in Low-Level driver LL_SPI_ReceiveData8 for STM32L0, STM32L4, STM32L5 and possibly others

Affected driver libraries: STM32Cube_FW_L5_V1.4.0, STM32Cube_FW_L4_V1.16.0, STM32Cube_FW_L0_V1.11.2 and possibly other device driver libraries based on the same SPI peripheralFile: stm32yyxx_ll_spi.h (Replace yy by L5, L4, F0, ...)Functions affected:...

SOfne.1 by Associate III
  • 3797 Views
  • 6 replies
  • 0 kudos

USB HID REPORT DESCRIPTOR SIZE

I have a report descriptor that consist of 456 bytes. The problem is : When i define USBD_CUSTOM_HID_REPORT_DESC_SIZE   456 in usbd_conf.h file, it raises overlow warning and my hid device no longer works. How can i define hid descriptor size bigge...

TDuma.1 by Associate
  • 1602 Views
  • 2 replies
  • 1 kudos

STM32F070F6 Bootloader USB DFU Mode not working.

I want to use STM32F070F6 usb dfu mode to upload program. The document An2606 page 53 says:If HSE is present and has a value of 24, 18, 16, 12, 8, 6, 4 MHz, the system clock is configured to 48 MHz with HSE as clock source. The DFU interface, USART1,...

0693W000001sOCMQA2.jpg
TYu.1951 by Associate II
  • 2026 Views
  • 2 replies
  • 0 kudos
ASpar.1 by Associate II
  • 3200 Views
  • 5 replies
  • 0 kudos

Resolved! Hardfault with Lwip Udp

Hello, I'm having trouble about use of lwip on Stm32h743. I'm using udp raw. I'm transmitting packet with 1ms period, there is no problem in sending/receiving. After 20-30 min, program is going to hardfault with 'Imprecise data access violation'. It ...

0693W000008xdWuQAI.png
Ey.1 by Associate II
  • 4258 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.