STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407DISCO IAP over Ethernet

Hey there,​following situation: lets say there is a product on the market based on a STM32F407 uC. This product has an ethernet connection over a PHY and it should be possible to update the firmware of the device over the ethernet connection.​As the ...

PUrsu.1 by Associate II
  • 1705 Views
  • 2 replies
  • 0 kudos

USB Device HUB class on f103

Is it possible to implement device HUB?(i want my f103 to appear as usb HUB to host PC)Like a compound device. Cant find any example for some reason.

VLuky by Associate II
  • 2369 Views
  • 4 replies
  • 1 kudos

Resolved! ERROR Transmitting data over USB .txstate!=0

Hi, I am trying to generate the usb_cdc FW, I generated the code using stm cube IDE,and the controller is stm32f070c6,i increase the heap size 0x400 and stack size 0x400,im taking the example from STM32Cube_FW_F0_V1.11.2\Projects\STM32072B_EVAL\Appli...

RKUMA.2 by Associate II
  • 1463 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 Nucleo-144 User USB

When I plug in the user usb port on the nucleo to my computer nothing shows up. I'd like to put it into DFU mode over usb so i can flash a custom bootloader.Thanks!

jkasper by Associate II
  • 1961 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.