STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I want to use TouchGFX with Azure RTOS

Hello.I want to use TouchGFX with AzureRTOS(Thread X).※board is STM32F769DISCO※TouchGFX Version is 4.16.0​I made stm32CubeIDE's project with TouchGFXDesigner.(selecting board→making Screen→Gnerate Code)​I opened this project with STM32CubeIDE.Next, I...

0693W000008zkhAQAQ.png 0693W000008zksNQAQ.jpg 0693W000008zkyBQAQ.jpg 0693W000008zkz4QAA.jpg
onosho by Associate II
  • 3062 Views
  • 4 replies
  • 0 kudos

STM32L412CBT6 controller interfacing with SPI-Fatfs-SD with battery power 2.8 volts. SD card detecting but f_open couldn't open a file and show an error. With same application working with regular power supply(2.8 volts)

I am Using STM32L412CBT6 controller in that the application working with a regular power supply 2.8 volts but with a battery the remianing modules(i2c/RTC) but in SPI F-open is not working

JRUDR.1 by Associate
  • 1565 Views
  • 1 replies
  • 0 kudos

STM32F7 lwip Ethernet connection problem

I've built an STM32F767 board on which I used the LAN8742 Phy chip as per the Nucleo board. The firmware is CubeMX derived with lwip and FreeRTOS used, and all IP addresses are static. If I connect my board to a 100 Mbit hub and a PC then I can somet...

Hello, I try to start with azure RTOS on a H723ZG and when looking at the examples (e.g. TCP-Client) it is completely different from code generated through CubeIDE from scratch. I hoped that generated code will be a working framework that I adjust/add.

CubeIDE makes a completely different file structure, some includes cannot be found "VOID" is written capital and causes an error, etc. I am completely new to RTOS, I did some bare metal HAL with CubeIDE and that worked quite well, but just started re...

GRand.1 by Associate II
  • 5787 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.