STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Bootloader Versions of STM32F42xxx/43xxx

Hello all,I have STM32F439 MCU.I use STM32CubeProgrammer to program the MCU through ST Bootloader.STM32CubeProgrammer writes:Bootloader protocol version: 3.1According to AN2606 (STM32 microcontroller system memory boot mode) the valid version for ST...

HAL_RCC_OscConfig ends in HardFault_Handler

HiI'm using a Nucleo-144 with a STM32F767ZI.I have included in my project FreeRTOS and FreeRTOS-IP although that may not be related with the problem, since the crash happens before reaching the initialisation of FreeRTOS.My problem seems to be that H...

EGonc.2 by Associate II
  • 1375 Views
  • 1 replies
  • 0 kudos

Resolved! SysTick_Handler and RTOS

Hello , I had started a project with STM32F410RB wish communicate with a keyboard and LCDActually i wrote my program that call SysTick_Handler from stm32f4xx_it.c to interact keyboard and detect if there is a button pressed and wrote caracter on LCD....

Ahajr.1 by Associate II
  • 3658 Views
  • 1 replies
  • 0 kudos

CPU Utilization using FreeRTOS

Hi I want to measure the CPU usage of the tasks running by FreeRTOS.I use the following code, but I see very inaccurate results.I want to use a sliding window, or even a timer.Is there a known solution or good practice to do so?I use FreeRTOS with ST...

deckhard by Associate III
  • 2214 Views
  • 1 replies
  • 0 kudos

Resolved! Is there any way to disable the RTC reset on STM32F476

The HAL RTC initialization routines for the STM32F476 unconditionally reset the clock toJanuary 1, 2000. I have a battery backup for the clock and do not want the clock reset on initialization.Has anybody found a way to do this within the CubeMX fra...

GJohn by Associate II
  • 2499 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.