STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FatFs F_Open Fails when Long File Name is enabled

Setup:STM32H743FreeRTOSFatFs8G SD card on SDMCC1 (FAT32 formatted)Hi,I have a problem with f_open which does not work when Long File Name is enabled (_USE_LFN = 2).f_open(&MyFile, "TEST.TXT", FA_CREATE_ALWAYS | FA_WRITE) == FR_OK) returns FR_INT_ERR....

Resolved! DFU Bootloader device not showing up in DfuSe Demo

I'm putting an STM32L4S into DFU bootloader mode by holding the BOOT0 pin high at power-up.That causes it to show up in WIndows 10 Device Manager under "Universal Serial Bus devices" as "STM32 BOOTLOADER". (It shows up under "Ports (COM & LPT)" as "U...

JWied by Associate
  • 7593 Views
  • 6 replies
  • 0 kudos

Resolved! AWS IoT with Nucleo-F767ZI?

So this is a related question to connecting through ethernet. I'm having trouble using my ethernet connection for AwS IoT. Are there any resources to do this? Most of what I found involved using wifi instead.

MBlanco by Associate II
  • 1210 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L072 UART bootLoader

I want to Implement the UART bootloader to the STM3272cz Microcontroller and flash the code with STM32cube programmer .I want to understand the STM32 cube programmer UART protocol used here for flashing the Bin file to the micro controller .Any sugge...

Sshan.1 by Associate II
  • 2221 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.