STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 SPI bootloader anomalies ?

Hello,I’m experiencing some difficulties trying to communicate with the embedded bootloader in SPI configuration.I have two separate Nucleo boards:-         NUCLEO-H753ZI-         NUCLEO-H743ZI2One of them is the master, the over is the slave (order ...

0693W00000JP29VQAT.png 0693W00000JP2AEQA1.png 0693W00000JP2AYQA1.png 0693W00000JP2BMQA1.png
ECA by Associate
  • 1193 Views
  • 0 replies
  • 1 kudos

Resolved! How to flash STM32 MCU using USB

Using IAR to develop software for and burn flash via USB on STM32 7B3I and Discovery eval boards.Need to develop my own Windows software to burn flash via USB on our own product.Am familiar with AN2606 [bootloader] and AN3156 [DFU] but neither appear...

Error in code generation for LwIP

Hi!I generate the CubeIDE project (FW v 1.3.0) for STM32H743ZI, but have an error. See full in "ethernetif.c"FreeMarker template error (DEBUG mode; use RETHROW in production!): The following has evaluated to null or missing: ==> SWIPdatas [in templat...

Alex_Doc by Associate
  • 1046 Views
  • 0 replies
  • 0 kudos

Is DMA possible with USB FS

I'm working on a STM32H750XB with USB. It works fine with the USB2_OTG_FS instance, but the speed is not reaching the maximum (only 875kB/s). I'm using the USB with diskio, FatFS and FreeRTOS.I'd like to enable DMA to make it faster, so I set hhcd.In...

BDELI.2 by Associate II
  • 2637 Views
  • 4 replies
  • 0 kudos

CDC USB receive with XMODEM

I'm using STM32F745. I would like to use the CDC USB to receive data from Tera Term using the XMODEM protocol. I can configure CDC_Receive_FS() to receive data for blocks of 64 bytes or less.  The procedure for this is well documented. XMODEM packet...

PKraj.1 by Associate II
  • 2193 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.