STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to install X-CUBE-CLASSB package on CUBEMX

Hello,I'm currently trying to use the "X-CUBE-CLASSB" package I'v found there : X-CUBE-CLASSB - Class B 60730-1 and 60335-1 Functional Safety Package with software expansion for STM32Cube - STMicroelectronics to do some watchdog, stack and flash secu...

TDele.1 by Associate III
  • 2699 Views
  • 1 replies
  • 0 kudos

Ethernet on ST STM32H747I Discovery board

Hello, I am working on the ST STM32H747I Discovery and I have a question regarding Ethernet. According to the ST documentation (https://www.st.com/resource/en/user_manual/dm00504240.pdf), some hardware modification is mandatory to manage Ethernet. Ho...

vlacr.11 by Associate II
  • 1454 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 Bootloader via SPI

I made a firmware download project using a factory bootloader according to AN4286. Everything works fine. I have only one ambiguity - in the description of the bootloader in AN2606 there is a picture on which the SCK signal is pulled-down to the grou...

0693W00000JPAHwQAP.png
ADoro.2 by Associate III
  • 1951 Views
  • 2 replies
  • 0 kudos

How to boot from and execute code from external Quad SPI flash memory on STM32H742 (STM32H7) using XiP model?

Hi all,we're planing to use an STM32H742 with external SDRAM (for data) and external Quad SPI flash.The Quad SPI flash shall hold the application binary - i.e. instructions, constants, etc. to be loaded at boot and all code to be executed.We'd like t...

mwb by Associate III
  • 7849 Views
  • 3 replies
  • 0 kudos

Resolved! f_mount returning FR_NOT_READY

Hi.I've been working on a project recently, and I've been having trouble with mounting an SD card. I've been getting FR_NOT_READY from f_mount function. Diving deeper into the code, I've found that SDMMC_GetCmdResp2 returns SDMMC_ERROR_CMD_RSP_TIMEOU...

fLicK by Associate
  • 4126 Views
  • 2 replies
  • 0 kudos

Boot Load configuration in STM32G070KB

Hi, I am using STM32G070KB controller. I tried to implement bootloader configuration via firmware as mentioned in document AN2606 and AN3155. But still its not entering boot mode. And also I need clarification for the "Execute BL_USART_Loop for USART...

AA.15 by Associate II
  • 2683 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.