STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to test Audio loop back (STM32f7508-DK)

Dear all,I have Stm32f7508-Dk ,I am trying to execute the BSP examples one by one Everything is ok but got stuck in Audio loopback As per instruction (Read Me file) we have to give input to Microphones U20 , U21 and we got the output in CN10 But i ca...

Ss.61 by Associate III
  • 1146 Views
  • 0 replies
  • 0 kudos

Unable to get DHCP working with STM32F407 + DP83848

Hi, I am unable to get DHCP working. I am using the DP83848 board with an STM32F4 Discovery board. I am using the STM32CubeIDE and so had the code generated, the DP83848 is working on RMII mode.When I enable or disable DHCP and connect it to my PC/la...

PFirm.1 by Associate II
  • 4053 Views
  • 7 replies
  • 0 kudos

DMIC and PDM to PCM Problem

Hi everyone, I have some question about DMIC and PDM to PCM audio output.My Board is STM32H735-dk board, and scenario is below:Using on board MP34DT01TR-M DMIC through PDM interface to SAI4 input PDM data (16kHz input, 1 channel)PDM data to PCM data ...

LKuo.2 by Associate
  • 2187 Views
  • 2 replies
  • 0 kudos

STM32CubeExpansion_Cloud_CLD_GEN_V1.0.0\Projects\STM32F769I-Discovery\Applications\Cloud\GenericMQTT\EWARM

I am able to successfully load the GenericMQTT project to STM32F769 discovery board. However, Up on selecting "Clear Connection" for the MQTT communication. The program is asking for CA certification. I believe CA certification is not required for Cl...

PMist.2 by Associate
  • 2108 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.