STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What could be causing the STM32L152 UART Rx interrupt to intermittently not fire when data arrives and interrupts are correctly configured?

Hello all,First off, I apologize that I am not able to provide code as everything I have been able to do reproduce this problem is proprietary. Given that, I am looking for advance debugging techniques for diagnosing this intermittent failure of the ...

BCogh.2 by Associate II
  • 4165 Views
  • 5 replies
  • 0 kudos

Resolved! How does Ethernet RX descriptor wrapping work on STM32H7?

My Ethernet driver is not wrapping as I expect.Section "61.10.1 Descriptor Overview" in RM0399 states that descriptors up to N-1 is owned by the DMA and the DMA continues to process descriptors until the Current Descriptor Pointer == Tail Pointer.In...

PWint by Associate III
  • 12917 Views
  • 14 replies
  • 2 kudos

STM32F745 USB communication fails

The project consists of STM32F745 MCU and a desktop application. The desktop application sends the data over USB CDC and receives the response back. The problem happens if large data chunks are being sent. What happens is that if several packets of l...

MDJ by Associate II
  • 2997 Views
  • 6 replies
  • 0 kudos

Function of ALERT pin(#19) for STUSB4500

In STUSB4500 datasheet, it says below for ALERT pin: Pin 19, B2, ALERT, OD, I2C interrupt, active low open drain, To I2C master, ext. pull-up.What does it mean - is the signal triggered when I2C command is sent from I2C master to STUSB4500?Thanks,...

WGao.1 by Associate II
  • 2524 Views
  • 5 replies
  • 1 kudos

FreeRTOS hangs on xQueueSend

My program hangs on xQueueSend call:if (xQueueSend(msg_queueHandle, (void *)&msg, 10) != pdTRUE) {When I step through the code, I see it reaches the xQueueGenericSend function but exits on the first line of that function where the following is called...

LMorr.3 by Senior II
  • 5356 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.