STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H745 USB CDC not working on M4 core

Hi,So with STM32CubeMX is it possible to generate a working CDC (VCP) for the M7 core.I'm unfortunately unable to generate one for the M4 core.What I did (for Nucleo-144):Selected STM32H745ZITxSystem Core->RCC: HSE to bypass mode.Connectivity->USB_OT...

Mvan .31 by Associate II
  • 3172 Views
  • 4 replies
  • 0 kudos

STM32H747 MP3 player (spiritMP3 decode)

Hello everyone,I'm on STM32H747, I use SpiritMP3 decode to play my music with an I2S DAC on the M7. This works very well.The problem is when I want to dialogue between the two Cores, I use Domain D3.But I have a "BusFault" which occurs after SpiritDe...

cVass.1 by Associate II
  • 1630 Views
  • 0 replies
  • 0 kudos

I need to Debounce Buttons with Press-Hold and Double-Tap detection. I'm using freeRTOS. Is it best to use a hardware timer interrupt, software freeRTOS timer or while(1) loop with osDelay(10) calls in a freeRTOS taks?

Using the while(1) with no timer seems like the simplest implementation and does not require a timer. Does using osDelay(10) inside a while(1) use more CPU than using software/hardware timer interrupt?

LMorr.3 by Senior II
  • 2834 Views
  • 2 replies
  • 0 kudos

Problem with adding extra charts to Azure Platform

Recently i imported example to Stm32CubeIDE and in this example i have only one chart. I don't have idea how to add extra charts. if anyone have idea how to add it please tell me or give me some explanations where i need to put or create datas in my ...

DJadc.1 by Associate II
  • 1882 Views
  • 3 replies
  • 0 kudos

Resolved! No response from bootloader after entering

Hello,I am trying to communicate with the bootloader by serial.Most of the times it works nice but sometimes it fails as I fail to enter the bootloader.To give a context, in order to enter the bootloader I set the rts of my FTDI high (this will set t...

0693W00000LyMK2QAN.png
JPatr.3 by Associate II
  • 2644 Views
  • 2 replies
  • 0 kudos

Bootloader on MCU

Hello everyone, i've been coding a bootloader for STM32L072 MCU's, i can download the binary file and write it into FLASH memory from specific address, all this process works, but at the time to jump to the code to be executed, it doesn't work...i ch...

0693W00000LyIBzQAN.jpg 0693W00000LyICdQAN.jpg
RComa.1 by Associate II
  • 2734 Views
  • 4 replies
  • 0 kudos

STM32G4 FDCAN HAL Driver Issue (v1.5.0)

The HAL_FDCAN_ErrorCallback is erroneously being called during every interrupt after a Protocol Error (PEA) occurs, even when no error exists during the interrupt. I believe this condition will occur for some of the other interrupts as well (ELO, WDI...

DAshb.11 by Associate
  • 2563 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.