STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO H753ZI LWIP Ethernet not working

Hi, I'm using the NUCLEO H753ZI board and trying to activate the Ethernet without success. I can't ping the board from a PC which is connected to the board by a switch. After configuring the ioc file by the CubeMX , creating a project and running by ...

yc.2 by Associate
  • 1613 Views
  • 1 replies
  • 0 kudos

hard fault in USB CDC host

I"m using my Nucelo-H745ZI-Q board with HAL for USB with CDC. I'm hitting the hard fault at the host project from the USBH_CDC_Transmit() function. On debuggin, I can see that the phost (USBH_HandleTypeDef type) ->ActiveClass->pData has no valid data...

Mr. AK by Associate III
  • 1013 Views
  • 0 replies
  • 0 kudos

Resolved! How to reference parameters set in .ioc file

I want my code to pick up a value set in the ioc project file, specifically:<project>.ioc | Pinout & Configuration | Software Packs | AZRTOS(M7) | ThreadX | Core | TX_TIMER_TICKS_PER_SECONDIs this possible? I see I can override this in tx_user.h, but...

'SMike by Associate III
  • 1456 Views
  • 1 replies
  • 0 kudos

to enable the threadx list

To know how much of stack is consumed,by my code and if i make any changes in my code how much of memory do i need ?and here in the figure we are not able to view the below listed content and also let us know how to enable the ThreadX list. 

0693W00000SvEPaQAN.png
Cv.1 by Associate II
  • 1982 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.