STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Two questions about HAL_GPIO_EXTI_IRQHandler

1- Using cubre-mx I enabled two IRQ lines, each generate its own ISRvoid EXTI0_IRQHandler(void){ HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_0);}andvoid EXTI15_10_IRQHandler(void){ HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_0);}Why HAL joint together both IRQ handlers ...

dhs by Senior
  • 4061 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L010F4P6 which pins are used by UART bootloader

Hello, I'm attempting to flash firmware to aforementioned microcontroller using STM32CubeProgrammer. I have connected ST-Link VCP port to PA2 and PA3 ports, and i can communicate with my application fine. I even erased flash memory so I could be sure...

tsma by Associate II
  • 4125 Views
  • 4 replies
  • 0 kudos

I have an issue with STM32L552 USB library. After sending an HID message once, the usb will send empty packets indefinitely (len=27, data len =0).

This is the data I recorded with WireShark. As shown in the picture, when I send HID packet once (len=91), the USB will send empty data packets indefinitely (len=27), then trying to send packets from host to device (out direction) will cause the tran...

YGree.2 by Associate II
  • 2743 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.