STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Board with some features similar to STLink

We have a new project and would like it to have some features similar to the STM32 on an STLink:a) Emulate a Thumbdrive using MCU FLASH and/or an external serial FLASH IC. The files should be accessible by both the STM32 and any PC connected to the U...

Paul1 by Lead
  • 2457 Views
  • 3 replies
  • 1 kudos

Bootloader doesn't work correctly (STM32L151) First program at 0x08033C00 , compiled with Mikroe, works correctly but I'm trying to add a STM32Cube bootloader so it can start it on one bank. It doesn't ... Thanks for help

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body *****************************************************************...

JFELI.13 by Associate III
  • 1673 Views
  • 4 replies
  • 0 kudos

The PC cannot detect USB device access after downloading the USB demo generated in STM32F411E-DISCO(MB1115-F411VE-D01) development board using STM32CUBMAX

USB DP and DM have no 1.5k pull-up resistance, which will not take effect after internal pull-up of DP or DM (DP or DM grounded), and the resistance value of current limiting resistance (R56 R58) is 12.5 Ω instead of the marked 22 ΩThe measured value...

0693W00000aHNy2QAG.jpg
lluo.3 by Associate
  • 1298 Views
  • 1 replies
  • 0 kudos

Resolved! "Generate Code" deletes 6 source files from an imported example (Nx_MQTT_Client) from ST's set. Manually replacing files temporarily fixes (until the next "Project->Generate Code".

I've a bunch of issues with STM32CubeIDE.To repeat the "Deleted Source Files" issue in STM32CubeIDE, running on a Mac M2 or Intel (not a Rosetta issue) under MacOS Ventura 13.x. STM32U5 board. Do the following:File->Import... General:Import STM32Cube...

AShap.3 by Associate III
  • 3059 Views
  • 5 replies
  • 0 kudos

i am having problem with keil uvision 5 and freertos

Helloi am having a problem with my own project, i create it with cubemx and use keil uvision 5 for the first build, but it gives a lot of errors, i don't know what to do next because i just learned how to use it it was 1 week ago.I use board : stm32f...

0693W00000YAFqNQAX.png 0693W00000YAFqhQAH.png 0693W00000YAFqXQAX.png
OWLchan by Associate III
  • 3081 Views
  • 4 replies
  • 0 kudos

STM32F107VCT6 and LAN8720 Ethernet Communicaton

Hello,currently we are working with easyMx Pro V7 Boards in Class and we are trying to get basic ethernet communication working. First time for everybody using stm32cubemx and HAL, even our teacher never used either one. Any Communication happening w...

MKräm.2 by Associate II
  • 3588 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.