STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Dual-bank boot not working on STM32L471 device

Hello,I am trying to use the dual-bank boot feature in order to safely upgrade the software application.The hardware configuration is the following:The mcu used is the STM32L471.The system bootloader version is v9.2BOOT0 pin = 0 so boot mode is set t...

JBlan.4 by Associate
  • 2363 Views
  • 2 replies
  • 1 kudos

PTP support in HAL drivers STM32H7

We have migrated our project from STM32F7 to STM32H7 MCU and found that there's no support for PTP IEEE 1588 protocol in MAC Ethernet driver (HAL). Here is a message written in stm32h7xx_hal_eth.c file:   -@- The PTP protocol offload APIs are not sup...

leshich-k by Associate II
  • 11315 Views
  • 16 replies
  • 0 kudos

USB Not recognized in stm32f429iit6

I am using stm32f429iit6 customized board . I have one hex file , when i debug that hex file in board its working fine and not giving any usb issues its shows stm virtual com port , But when i write program for same board its giving the USB driver is...

pshin.2 by Associate II
  • 2197 Views
  • 4 replies
  • 0 kudos

Resolved! The questions about stm32f1 Usb-hid.The libs from TM32 USB-FS-Device Lib V4.1.0' Custom HID#Insert get report in RESULT CustomHID_Data_Setup/usb_prop.c

The original CustomHID_Data_Setup function :RESULT CustomHID_Data_Setup(uint8_t RequestNo) { uint8_t *(*CopyRoutine)(uint16_t);   if (pInformation->USBwIndex != 0)   return USB_UNSUPPORT;   CopyRoutine = NULL;     if ((RequestNo == GET_DESCRIPTOR)   ...

0693W00000aHo8XQAS.png

Resolved! STM32G0 erasing bank2

I am using a stm32g0b1ret with stm32cubemx package 1.6.1 .The symptoms are:On deletion of pages I receive a signal 0 in the debugger, but the pages do get erased eventually. (I use HAL_FLASHEx_Erase)On the first flash write I get an error with goes t...

JRS by Associate III
  • 4290 Views
  • 4 replies
  • 0 kudos

Resolved! X-CUBE-AZRTOS-L4 not working in CubeMX

Installed the X-CUBE-AZRTOS-L4 package with the CubeMX "Install software packages" function. Looks like it is installed.Starting a new Project with an STM32L4 device does not show the Azure RTOS Middleware options. Bug or what I am doing wrong?!

0693W00000aHsnPQAS.png 0693W00000aHsocQAC.png

Resolved! STM32G071 UCPD Dead Battery pins does not work.

I have STM32G071 MCU to control a USB Type C hub and I want to use VBUS Powered sink in the application. I have connected Dead Battery pins to their respected CCx pins. It supposed to act as a sink when there is no power but when I connect the type c...

Cagatay by Associate II
  • 3493 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.