STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have an STM32H743. I am trying to configure a Layer 4 inverse filter on destination port . My intention is to allow all broadcast traffic except for one that has a particular destination port.

I am configuring the following control registers.  heth->Instance->MACCR |= ETH_MACCR_IPC; // INVERSE MATCHING heth->Instance->MACPFR |= ETH_MACPFR_IPFE; heth->Instance->MACL3L4C0R |= 1<<21;//ETH_MACL3L4C0R_L4DPIM0; heth->Instance->MACL3L4C0R |= 1<<2...

ABuce.1 by Associate
  • 1247 Views
  • 1 replies
  • 0 kudos

DRD Settings for NUCLEO-G071RB and X-NUCLEO-DRP1M1

I would like to use NUCLEO-G071RB and X-NUCLEO-DRP1M1 to Source,UFP my USB devicesWhen the USB device side is set as Source, the role of data is DFP.​I used the DR SWAP command to change from DFP to UFP.But there was no sample code in x-cube-tcpp_v4....

forst by Associate III
  • 1652 Views
  • 1 replies
  • 0 kudos

CANBUS communication stops after a while. Is there any solution to make up. (e.g. reset communication)?

Hello everyone. I use STM32F4 to transmit CANBUS messages. When i connect Can High and Can Low lines to CAN-USB transformer i see messages coming to computer but after a short while the communication between MCU and computer stops. If i reset the MCU...

Resolved! Hi i am Roberto, For my project i need to update the firmware from USB port so i need to use internal bootloader. The MCU is contained into a close box so i can't set BOOT0 pin manually. Do you have any idea ?

My idea is that:I want to put a resistor and a capacitor on BOOT0 pin. When normal code is running and i will go to update the firmware, i will send a command to USB. When MCU will receive this command, MCU will set BOOT0 pin to high state and charge...

RCola.2 by Associate II
  • 3375 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.