STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

declaring variables with ram address

I declared some test variable like,unsigned short *testvar= (unsigned short *)0x20020074;unsigned char *testvar1[4] = {(unsigned char *)0x20020076,(unsigned char *)0x20020077,                                                  (unsigned char *)0x200200...

madhavi U by Associate II
  • 1456 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F4 USB "Hello world" example?

Hi, i am trying to use USB VCP device on STM32F401. Is there a example available for this? Optimally, if it ends with something like the "Hello World" display in the terminal. My goal is to replace FTDI with internal USB in STM.Thanks

PHude.1 by Associate III
  • 14703 Views
  • 17 replies
  • 1 kudos

Resolved! LWIP with STM32F769

Posted on May 21, 2018 at 17:07I want to use the ETH port to communicate with other devices. I started by creating a project in CubeMX for the STM2F769I-Disc board. I simply added the LWIP and the ETH port (as RMII) and set a specific IP address (wh...

Rick MC by Associate III
  • 4752 Views
  • 8 replies
  • 2 kudos

USBPD need for USBX communication

Hello, I'm using the Evaluation board B-U585I-IOT02A for the STM32U585, and I'm playing around with the USB communication using the example "Ux_Device_HID_CDC_ACM". However, I'm not sure to fully understand the use of the middleware USBPD, which in m...

fs.clar by Associate
  • 2188 Views
  • 2 replies
  • 2 kudos

Resolved! AWS Iot Core Connection / Project Build Error ( B-L4S5I-IOT01)

B-L4S5I-IOT01 보드를 사용하고 있으며, AWS Iot에 연결하는 과정을 따라하고 있습니다. aws-demo 빌드시 오류가 발생하면 결함을 발견할 수 있는 방법이 도움이 되었습니까? 미리 감사드립니다. https://catalog.us-east-1.prod.workshops.aws/workshops/b5857416-f2f6-4188-8562-053ec5f983ef/en-US/lab-0  > 불러오기 링크 >오류가 발생한 화면 (x-c...

빌드 에러 사진.png
dongkey by Associate II
  • 3260 Views
  • 4 replies
  • 0 kudos

Resolved! Problem with custom bootloader and STM32F042 (Solved)

Dear Friends, Edited:I have a bootloader that I made via I2C through the mailbox of an ST25DV04.The bootloader works fine, it is able to save in the flash the whole content of the hex file (valid data).I have added vector table remapping in my "blink...

RamiroGJ by Associate II
  • 1912 Views
  • 1 replies
  • 0 kudos

STM32 C011

Hi,I am going to be a part of a firmware development using STM32C0 series. Can I able to use ADC input which is input power supply as EXT Interrupt  to wake up from sleep mode?How can be it assigned in ?Please Can anyone give an idea?

meena by Associate III
  • 1788 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G070RBT6 I2C communication with ESP32 S3 C1 devkit

Hi, I am new to STM32, I am trying the i2c communication between stm32 and esp32. I am using STM32 as slave and ESP32 as Master. I am using Arduino IDEI connected stm32  PB6-SCL, PB7-SDA to esp32  GPIO21-SDA, GPIO19-SCL.i was not getting any response...

RamyaD by Associate II
  • 4895 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.