STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LWIP PBuf Queue?

Hello,I have a STM32 sending a packet a second, up to 25 UDP packets, to another STM32 whose role is to echo these packets back to the sending STM32.Inside the packets is a value which I increment after every transmission.I've noticed that at the ori...

###### by Senior II
  • 2860 Views
  • 2 replies
  • 0 kudos

I need help to Modbus TCP/IP

Hi everyone, I am trying to write modbus tcp/ip server(slave) with stm32h7. I know the Modbus working logic and I have worked with Modbus RTU many times before, but I am unfamiliar with the ethernet layer. I couldn't find a resource to write modbus t...

Matt_ by Associate II
  • 4738 Views
  • 6 replies
  • 0 kudos

Design guidelines for embedded applications

I've been doing a lot of embedded coding lately. I'm not a very experienced developer and I have been trying to develop a set of design guidelines to help me up the learning curve.  I'd appreciate hearing what experienced embedded developers use for ...

magene by Senior II
  • 4392 Views
  • 4 replies
  • 2 kudos

Resolved! HAL_delay() issue infinite loop

I am using a nucleo-f767zi to control a reverdi tft display.The project in CUBEMX ide is using freertos and there for the time base is changed from systick to TIM6.I am trying to task enable sequence for the screen but i see that i am stack in an inf...

Kyrpav by Associate III
  • 7938 Views
  • 7 replies
  • 0 kudos

No rule to make target

I upgraded my project to the latest IDE and TouchGFX.  I opened the IOC file to change a setting and now the project doesnt compile with the following errors. Before opening the IOC and generating new code, the project compiled just fine. Here is wha...

JWall.1 by Associate II
  • 1004 Views
  • 0 replies
  • 0 kudos

STM32H7 USB DMA CDC does not work properly.

Hi everyone. I have an issue with USB transmission in DMA mode (USB_OTG_HS, internal PHY, FullSpeed 12MBit/s). I am using a Cube generated project for STM32H743IGT6. If I disable DMA - it works fine. But when I enable DMA USB enumerates on PC and all...

Yaroslav1 by Associate II
  • 1624 Views
  • 1 replies
  • 0 kudos

STM32F723VEY6TR rise time information?

Hello, we are working on a project using the STM32F723VEY6TR and have been curious about rise time information, especially so regarding the rise time information for SPI.I have found some information on page 174 in the following datasheet:https://www...

BGilm.1 by Associate
  • 1462 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.