2023-08-19 10:48 AM - edited 2023-08-19 10:53 AM
I've been having this problem where I configure my STM32F303VCT6 to send out 8 bits but the CLK sends out 16 cycles. I already tried casting the data as proposed on other forum posts but it doesn't work for me. Does anyone see the problem?
- - - Library Code - - -
void LLD_SPI_INIT(SPI spi){
uint32_t *RCC_APB2ENR = (uint32_t*)0x40021018; //RCC Register for AHB which holds clock to SPI peripheral
//Configure SPI pins
LLD_GPIO_INIT(spi.MISO);
LLD_GPIO_INIT(spi.MOSI);
LLD_GPIO_INIT(spi.SCK);
LLD_GPIO_INIT(spi.CS);
LLD_GPIO_CONFIG(spi.MISO);
LLD_GPIO_CONFIG(spi.MOSI);
LLD_GPIO_CONFIG(spi.SCK);
LLD_GPIO_CONFIG(spi.CS);
LLD_GPIO_SET_PIN(spi.CS, 1);
//Enable clock for SPI pin
*RCC_APB2ENR |= (1 << 12);
}
void LLD_SPI_CONFIG(){
uint32_t *SPIx_CR1 = (uint32_t*)0x40013000; //SPI control register 1
uint32_t *SPIx_CR2 = (uint32_t*)0x40013004; //SPI control register 2
//Disable SPI
*SPIx_CR1 &= ~(0x01 << 6); //Clear bits
//Baud rate
*SPIx_CR1 &= ~(0x07 << 3); //Clear bits
*SPIx_CR1 |= (0x03 << 3); //Set bits
//Master configuration
*SPIx_CR1 |= (0x01 << 2); //Set bits
//Set SSI bit
*SPIx_CR1 |= (0x01 << 8); //Set bits
//Set SSM bit
*SPIx_CR1 |= (0x01 << 9); //Set bits
//Clock is usually low
*SPIx_CR1 &= ~(0x01 << 1); //Clear bits
//On upcoming clock flank
*SPIx_CR1 &= ~(0x01 << 0); //Clear bits
//RXNE when FIFO level is greater than 8 bits
*SPIx_CR2 |= (0x01 << 12); //Set bits
//Send 8 bits
*SPIx_CR2 &= ~(0x0F << 8); //Clear bits
*SPIx_CR2 |= (0x07 << 8); //Set bits
//Enable SPI
*SPIx_CR1 |= (0x01 << 6); //Set bits
}
void LLD_SPI_SEND_8BITS(SPI spi, uint8_t *data, uint32_t size){
uint32_t *SPIx_DR = (uint32_t*)0x4001300C; //SPI data register
uint32_t *SPIx_SR = (uint32_t*)0x40013008; //SPI status register
LLD_GPIO_SET_PIN(spi.CS, 0);
for(int i = 0; i < size; i++){
//Wait until TXE bit is set
while(((*SPIx_SR >> 1) & 0x01) == 0);
//Load data into Data Register
//*(volatile uint8_t*)&SPIx_DR = data[i]; //SPI doesnt send anything
*SPIx_DR = data[i];
}
LLD_GPIO_SET_PIN(spi.CS, 1);
}
- - - Main - - -
pindef LCD_EN = {GPIOC, 0, Output, PushPull, LowSpeed, NoUpDown, 0}; //Backlight
pindef LCD_RS = {GPIOC, 1, Output, PushPull, LowSpeed, NoUpDown, 0}; //Command/Read low = command, high = read
LLD_GPIO_INIT(LCD_EN);
LLD_GPIO_CONFIG(LCD_EN);
LLD_GPIO_SET_PIN(LCD_EN, 1);
LLD_GPIO_INIT(LCD_RS);
LLD_GPIO_CONFIG(LCD_RS);
LLD_GPIO_SET_PIN(LCD_RS, 1);
pindef MISO = {GPIOA, 6, Alternate, PushPull, MediumSpeed, NoUpDown, 5};
pindef MOSI = {GPIOA, 7, Alternate, PushPull, MediumSpeed, NoUpDown, 5};
pindef SCK = {GPIOA, 5, Alternate, PushPull, MediumSpeed, NoUpDown, 5};
pindef CS = {GPIOF, 10, Output, PushPull, MediumSpeed, NoUpDown, 0};
SPI SPI1 = {MISO, MOSI, SCK, CS};
LLD_SPI_INIT(SPI1);
LLD_SPI_CONFIG();
/* Loop forever */
while(1){
delay_us(100000);
//LCD command
uint8_t data[] = {0x28};
LLD_GPIO_SET_PIN(LCD_RS, 0); //Command
LLD_SPI_SEND_8BITS(SPI1, data, 1);
LLD_GPIO_SET_PIN(LCD_RS, 1); //Read
}
- - - Oscilloscope - - -
Solved! Go to Solution.
2023-08-19 11:36 AM
Change
uint32_t *SPIx_DR = (uint32_t*)0x4001300C;to
volatile uint8_t* SPIx_DR = (volatile uint8_t*) 0x4001300C;
2023-08-19 10:54 AM
Write DR with byte width not word
2023-08-19 10:57 AM
I'm sorry I'm pretty new to programming so I don't understand what you're saying.
What should I change in my code?
2023-08-19 11:36 AM
Change
uint32_t *SPIx_DR = (uint32_t*)0x4001300C;to
volatile uint8_t* SPIx_DR = (volatile uint8_t*) 0x4001300C;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.