STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADC STM32L152 with 25 channel

 Hi all,I am doing a project and need up to 25 ADC channels to read current from HAL ACS712 sensor,I have never read so many ADC channels.I saw that the STM32L152VET6 supports 25 ADC channels, so I chose it.I have a problem when configuring with ST32...

Hoi_0-1694250437569.png
Hoi by Associate II
  • 2209 Views
  • 3 replies
  • 1 kudos

STM32F070CBT6 jump to System Memory DFU

Posted on December 08, 2016 at 17:50 I'm trying to jump from an application to the DFU System Memory Bootloader. According toAN2606 this should work with my processor and the System Memory should start at address0x1FFFC800. I'm using an e...

Resolved! STM32G474RE opamps bias

Hello,I am thinking of buying an nucleo-g474re for 3-channel DMA sampling from the ADCs. Before I acquire one, I'd like to know if it can fit my use case. There are three analog input sources. Each one ranges from -100mV to +100mV. Is it possible for...

avbotz by Associate
  • 2927 Views
  • 4 replies
  • 2 kudos

Resolved! Using STM32 examples on custom boards

Hello,I have made a custom board using the STM32WB55CEU6 chip and I would like to try out some examples that are available from ST. My problem is that these examples are made for STM32WB55CG and I can't find an easy way to change target of these exam...

dryet by Associate II
  • 2717 Views
  • 1 replies
  • 0 kudos

stm32g0b1 Intern bootloader by FDCAN

HelloI have two boards master(stm32h743) and slave (stm32g0b1).I am trying to use FDCAN intern bootloader to update stm32g0b1.I have the upgrade file (bin file) for stm32g0b1 saved inside SD-card that the master board has access to.Stm32g0b1 starts f...

Resolved! I2C master and slave same time

Can I use STM32F401RCT6 to be I2C master and slave at the same time?1: For the Master, I use I2C1 -> pin PB6 and PB7, I will read data from the current sensor ICs.2: For Slave, I use I2C3 -> pin PA8 and PC9, I will send and receive data from another ...

Hoi_0-1694422529454.png
Hoi by Associate II
  • 2096 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.