2023-09-10 11:14 PM
Hello.
I have some questions while testing a product using the 107MCU.
As the title suggests, when I set up FreeRTOS and create a task, the commonly used callback functions cannot be called:
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi) void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi) void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi) void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
If I remove the task creation function, it operates normally.
Do you know why this is happening?
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.