2023-11-07 6:14 PM
Hi,
I am trying to setup USB CDC as virtual COM port on STM32L151. I just enabled it through cubeMX and connected the wires. Windows keep saying device not recognized.
I just did the exact same thing with STM32G431. An empty project with just USB CDC enabled through cubeMX. The exact same wiring and it works.
I am quite confused and lost. Looked a lot in the web but so far no solution.
Does anyone know what could be the difference between these two micro that one works and the other not? Or where should I look?
Thank you
2023-11-08 12:12 AM
Hello @HKaze.2 ,
Have a look to this FAQ: USB device not recognized, it may help you.
You can refer to the CDC example in the STM32CubeL1 firmware package and get inspired from the available one:
STM32Cube_FW_L1_V1.9.0\Projects\STM32L152D-EVAL\Applications\USB_Device\CDC_Standalone
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-08 3:58 AM
The 'L1 USB requires an external 1k5 pullup on DP, similarly to 'F1 (see e.g. STLinkV2 schematics).
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.