STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FP-AUD-AEC1 on NUCLEO-F446RE

Hi, I'm trying to get the FP-AUD-AEC1 v1.2.0 acoustic echo cancellation demo application to work.I have a NUCLEO-F446RE board, an X-NUCLEO-CCA02M2 expansion board and an X-NUCLEO-CCA01M1 expansion board.I programmed the NUCLEO-F446RE board with the S...

PascalB by Associate
  • 3426 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H5 MCU package download error

Hi,I cannot download the latest packeges for the H5 MCU-s. From cube IDE I got the error as the attached picture. I got error also from browser from here: https://www.st.com/en/embedded-software/stm32cubeh5.html

MGerz by Associate II
  • 2377 Views
  • 2 replies
  • 0 kudos

Project feasible (DMA-I2S-SPI-SDIO)?

Hi,I was wondering if I can get some feedback on the following project, mainly if the requirements I have are feasible?I was thinking on using an STM32F4 or STM32F7. The project consist of the following parts:An external DAC that is controlled throug...

User10 by Associate II
  • 3143 Views
  • 4 replies
  • 2 kudos

Resolved! STM32L412RB

we're using STM32L412RB microcontroller and it has 2*12 bit ADC and our project requires 8 bit resolution, in this controller can we configure the resolution from 12 to 8 bits?

HTTPS client using STM32F429ZI

Hi,I am attempting to implement HTTPS on STM32 using CubeIDE, but it seems that there are no libraries available for this purpose. Is it possible to achieve this on STM32 using wolfSSL or any other alternative?This is for study purposes; therefore, i...

sonysev by Associate
  • 4682 Views
  • 4 replies
  • 1 kudos

STM32CubeMonitor-UCPD cannot connect with GUI

Hello,I am following this guide, https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Dual_Role#Clear_the_pinout, and am unable to get the device to appear in the board selection window of the UCPD monitoring soft...

NMartin by Associate III
  • 2944 Views
  • 4 replies
  • 0 kudos

pragma optimize=speed high with noops

I wanted to understand the behavior of software that I see.There is a macro that has a few no-opsThere is #pragma optimize=speed high in the codeIs my understanding correct that #pragma is enforced after preprocessor expands the macros?So I think bec...

coolname by Associate II
  • 1943 Views
  • 1 replies
  • 0 kudos

Liv4FTR IRNSS / NAVIC Firmware

Hi,In the datasheet --> https://www.mouser.com/datasheet/2/389/teseo_liv4f-3011072.pdf"IRNSS constellation ready"&"2.5 IRNSSThe Teseo-LIV4F is ready for IRNSS using a dedicated firmware." is mentionedFrom where can we get the IRNSS / NAVIC supporting...

mvk by Associate
  • 1445 Views
  • 1 replies
  • 0 kudos

CubeMX USB CDC Problem

Posted on August 18, 2017 at 11:27i am working with STM32F446RE in a custom board and my Cube MX version is 4.22.0 and CubeF4 version is 1.16.0i want to send large data from USB HS in CDC class to PC.i don't change any cube parameters except Enable ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.