STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo H503 : USBx

Hello , Import example code from package en.stm32cubeh5-v1-1-0\STM32Cube_FW_H5_V1.1.0\Projects\NUCLEO-H503RB\Applications\USBX\Ux_Device_CDC_ACMand Run the example using STMcubemx IDE Gives hard fault error when call function ux_dcd_stm32_initialize(...

pooja by Associate II
  • 1531 Views
  • 1 replies
  • 0 kudos

Resolved! UART DMA multiple transmissions/receptions failure

Hi all,I'm facing an issue that has already been discussed several times in this and others forum, I attempted all the proposed solutions I could find but without success.I want to read the characters user inputs via Tera Term and store them in a buf...

Beppe101 by Associate III
  • 3246 Views
  • 5 replies
  • 4 kudos

STM32F373 SDADC stabilization never ends

I am working withe the STM32F373 SDADC on the STM32F373_EVAL board.When selecting the internal reference voltage (hsdadc1.Init.ReferenceVoltage  = SDADC_VREF_VREFINT1) ,the function HAL_SDADC_Init() will get stuck at while((hsdadc->Instance->ISR & SD...

BPutt.1 by Associate II
  • 929 Views
  • 0 replies
  • 0 kudos

USBX UAC2 playback issues

Looking for a bit of advice.I'm developing a full speed USB audio class device using USBX and ThreadX. So far, I've successfully rebuilt the provided example written for the H743 eval board on an F407 Discovery board. The device enumerates correctly ...

m_g by Associate II
  • 1867 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.