STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to set default PHY stm32wb55rg

We're using the stm32wb55rg as the core MCU in a project requiring decently high-frequency BLE notifications to a mobile device (100Hz update rate on the characteristic). In testing this I found that, with default settings, the bluetooth connection w...

Redrield by Associate
  • 2083 Views
  • 1 replies
  • 1 kudos

STM32 RNDIS USB device disappear after a while

Hello,I'm opening a new conversation to address another issue(Issue with VCP and RNDIS ). Previously, I successfully implemented RNDIS on an MCU, and I can see the Remote NDIS based Sharing Interface in the device manager. However, after about 20 sec...

dnj_0-1701342901354.png dnj_1-1701343277723.png dnj_2-1701343651192.png
dnj by Associate III
  • 1835 Views
  • 0 replies
  • 0 kudos

Resolved! USB RNDIS + USB VCP on STM32L462

Hi, I would like to enable RNDIS + VCP on this MCU. Is there an option to do that?I do not know how to enable only RNDIS for this MCU too (I do not see this on drop down with Class for FS IP).

dnj_0-1700574311825.png
dnj by Associate III
  • 6932 Views
  • 9 replies
  • 4 kudos

FreeRTOS Priority Issue with ETH / LwIP (f746)

I develop a FreeRTOS / LwIP based application which throws a configASSERT error because of a bad priority.Only when the Nucleo is connected to the LAN, the debugger gets stuck at:Line 744 of port.c (FreeRTOS source)configASSERT( ucCurrentPriority >= ...

0693W000008yeQzQAI.png 0693W000008yeR4QAI.png
Mnemocron by Associate III
  • 3027 Views
  • 4 replies
  • 0 kudos

STM32H7 Ethernet With FreeRtos and LWIP

Hello,using the STM32H7 Ethernet with FreeRtos and LWIP results in not sent packages as the Optimization is Turned higher than -O0. The lwip Stack ,for example, tries to send UDP Packages. Those packages never leave the STM32 and UDP data packets ar...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.