STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 Hal Ethernet Use of LWIP_MEMPOOL_DECLARE

Not sure if this is a bug or something I do not completely understand, but in the generated ethernetif.c file (HAL V1.9.0) there is the line:LWIP_MEMPOOL_DECLARE(RX_POOL, 10, sizeof(struct pbuf_custom), "Zero-copy RX PBUF pool");Which always uses, if...

JRS by Associate III
  • 13425 Views
  • 18 replies
  • 6 kudos

Bug in STM32WBXX_HAL_RTC

As of version 1.12.0, HAL_RTC_Init uses a macro named __HAL_RTC_IS_CALENDAR_INITIALIZED. It is defined as follows:#define __HAL_RTC_IS_CALENDAR_INITIALIZED(__HANDLE__) ((((RTC->ISR) & (RTC_ISR_INITS)) == RTC_ISR_INITS) ? 1U : 0U)I suppose it should r...

LWChris by Associate III
  • 2639 Views
  • 4 replies
  • 0 kudos

Resolved! STM32U5A5 HS Example

Hi guys.Im trying to port an application from STM32F4 over to U5A5.On the F4 i used an external usb hs phy. I was extremely delighted to find out that the new U5 has an integrated hs phy, only to see that:1. No more ST stack in cubemx. Ok, found a gi...

PMera.1 by Associate III
  • 2276 Views
  • 1 replies
  • 0 kudos

[STM32H753] CRYP FIFOs flush for AES

Hello,According to the Reference Manual v8 of STM32H753 one has to to flush the FIFO to perform a cipher operation:  The STM32Cube source code example is not doing this flush for AES-GCM (it does the flush for DES and TDES)I implemented my code like ...

Gpeti_0-1701083358772.png
Gpeti by Senior II
  • 1629 Views
  • 1 replies
  • 0 kudos

ADC_STm32G0

hi..I have tried all the ways to read ADC values as I found that using PA11(ADC_IN15) and PA12(ADC_IN16) is the issue.I tried setting up non configured mode  with polling and also DMA (as per CubeG0 examaples) I couldnt able to read the values. Can a...

meena by Associate III
  • 1348 Views
  • 1 replies
  • 0 kudos

Resolved! ADC_Reading same values

I have programmed STMG030k8T6 MCU in a prototypeChannels used ADC_IN_0 as T_sense  ADC_IN_15 AS BattMonif I am calling any one of the function I am getting exact values what i measure in hardwareBut if i called them both only reading values from CH 0...

SRAM11_0-1701103048704.png SRAM11_1-1701103092703.png SRAM11_2-1701103141318.png
SRAM.11 by Associate III
  • 2715 Views
  • 2 replies
  • 0 kudos

OV7670 FIFO Camera Wiring

Hi,I am working on the OV7670 FIFO camera module with NUCLEO-H745ZI-Q board. My purpose is taking the image data and saving SD card via BMP format. I tried a lot of codes from github and Youtube but it didn't work. Finally I found the Udemy course vi...

koksoybedirhan_0-1700738467779.png

_exit() implementation in syscalls.c wrong?

Looking at the file "syscalls.c" I found the following line:The implementation of "_exit()" calls "_kill(status, -1)".Shouldn't it be "_kill(-1, status)" instead?Note: Because "_kill()" is implemented as dummy by default, this line has no effect unle...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.